Other Parts Discussed in Thread: TM4C1294KCPDT, ADS8598S, TUSB422, EK-TM4C1294XL
We have had two TM4C129X development boards and a prototype board of our own design fail with what seems to be a short on the 3V3 rail by the processor. The dev kit uses the TM4C129XMCZAD processor and our prototype uses the TM4C1294KCPDT variant of the processor.
In each case the systems have been powered from USB ports. In the case of our prototype board I have a VBUS current monitor on the device and know that it was usually drawing about 40mA which agrees well with the datasheet and the work we were doing with the processor. We have a third dev kit which has been running with heavy use for a number of months without failure. We have been using our prototype board heavily for about a month. All of the devices worked correctly for several week to a few months before failing.
Our worry is that there is a failure mode with these processors that we are not aware of and that will impact customer units. We haven't been able to determine any proximate cause. ESD is a possibility, but seems unlikely in a populated system and more unlikely given that the failure mode seems to be the same in each case. Could it be a 3V3 supply related issue? That seems unlikely in the context of a development board.
So, is this a known issue?
If so, is there standard mitigation for the issue or do we change our design to use a different processor family (probably from a different manufacturer)?