Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS1224: CAN Tx pin is always high

Part Number: TMS570LS1224

Hi,

I have referred to CAN tutorial on ti website and written the code accordingly. But the transmit pin of DCAN1(2,3 also) is always when CAN Transmit is performed. Please give me some suggestion. I have referred the following link https://e2e.ti.com/support/microcontrollers/hercules/f/312/p/638525/2355828?tisearch=e2e-sitesearch&keymatch=CAN%20transmit%20not%20working%20on%20TMS570ls1224#pi320995filter=all&pi320995scroll=false but the problem is not yet solved.

/** @file sys_main.c 
*   @brief Application main file
*   @date 11-Dec-2018
*   @version 04.07.01
*
*   This file contains an empty main function,
*   which can be used for the application.
*/

/* 
* Copyright (C) 2009-2018 Texas Instruments Incorporated - www.ti.com 
* 
* 
*  Redistribution and use in source and binary forms, with or without 
*  modification, are permitted provided that the following conditions 
*  are met:
*
*    Redistributions of source code must retain the above copyright 
*    notice, this list of conditions and the following disclaimer.
*
*    Redistributions in binary form must reproduce the above copyright
*    notice, this list of conditions and the following disclaimer in the 
*    documentation and/or other materials provided with the   
*    distribution.
*
*    Neither the name of Texas Instruments Incorporated nor the names of
*    its contributors may be used to endorse or promote products derived
*    from this software without specific prior written permission.
*
*  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
*  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
*  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
*  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
*  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
*  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
*  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
*  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
*  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
*  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
*  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/


/* USER CODE BEGIN (0) */
/* USER CODE END */

/* Include Files */

#include "sys_common.h"

/* USER CODE BEGIN (1) */
#include "can.h"
#include "gio.h"

/* Include ESM header file - types, definitions and function declarations for system driver */
#include "esm.h"

#define  D_SIZE 9
unsigned int i=0;
uint8  tx_data[D_SIZE]  = {'H','E','R','C','U','L','E','S','\0'};
uint8  rx_data[D_SIZE] = {0};
uint32 error = 0;

uint32 checkPackets(uint8 *src_packet,uint8 *dst_packet,uint32 psize);
/* USER CODE END */

/** @fn void main(void)
*   @brief Application main function
*   @note This function is empty by default.
*
*   This function is called after startup.
*   The user can use this function to implement the application.
*/

/* USER CODE BEGIN (2) */
/* USER CODE END */

int main(void)
{
/* USER CODE BEGIN (3) */

    /* initialize can 1 and 2   */
    canInit(); /* can1 -> can2 */
    gioInit();
    gioSetDirection(gioPORTB,0x0F);

   //while(1)

    /* transmit on can1 */
      canTransmit(canREG1, canMESSAGE_BOX1, tx_data);
      for(i=0;i<=65000;i++);

    /*... wait until message receive on can2 */
//    while(!canIsRxMessageArrived(canREG2, canMESSAGE_BOX1)){
//        canGetData(canREG2, canMESSAGE_BOX1, rx_data);  /* receive on can2  */
//        gioSetBit(gioPORTB,2,1);
//    }
//
//
//    /* check received data patterns */
//    error = checkPackets(&tx_data[0],&rx_data[0],D_SIZE);
//    if(error!=0){
//        gioSetBit(gioPORTB,1,1);
//    }
//
//    /* ... run forever */
      while(1);

/* USER CODE END */

    return 0;
}


/* USER CODE BEGIN (4) */
/** @fn checkPackets(uint8 *src_packet,uint8 *dst_packet,uint32 psize)
*   @brief check two buffers and report error
*
*/
uint32 checkPackets(uint8 *src_packet,uint8 *dst_packet,uint32 psize)
{
   uint32 err=0;
   uint32 cnt=psize;

   while(cnt--)
   {
     if((*src_packet++) != (*dst_packet++))
     {
        err++;           /*  data error  */
     }
   }
   return (err);
}

/* USER CODE BEGIN (4) */
void gioNotification(gioPORT_t *port, uint32 bit){
    return;
}

void esmGroup1Notificatoin(int bit){
    return;
}

void esmGroup2Notificatoin(int bit){
    return;
}
void canErrorNotification(canBASE_t *node, uint32 notification){
    return;
}
void canMessageNotification(canBASE_t *node, uint32 messageBox){
    return;
}
/* USER CODE END */

  • Hello Phaniraj,

    Have you initialized the CAN module correctly?
    1. The default CAN TX state after CAN module initialization is HIGH (recessive)
    2. If there is no CAN transceiver, after you send message to CAN bus, your CAN will go BUS-OFF immediately due to massive occurrence of CAN bus errors, and CAN TX is recessive (HIGH). Please check the error counters which is 0xF8.
    3. During device reset, the CAN signals are pulled HIGH
    4. If the CAN module is configured to silent mode, the CAN TX is become HIGH
    5. If the CAN pin is configured as GIO mode, the CAN signal may be at HIGH state (based on CAN TX IO setting)
  • Hi QJ Wang,

    Thanks for your reply. After going through the 5 points above the problem is identified in CAN transceiver. Now CAN transmit is working.

    Best regards,

    S Phaniraj

  • Nice to know that the issue has been solved. I will close this thread. Thanks