Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
Hi,
When we configure the RTI of the TMS570, a reset occurs.
The initialisation procedure is provided herafter.
Could you help us to find what kind of mistake we have done?
Regards
Benoit
procedure MARTM_INI_RTI_INIT (pU32_RTI_FREQ_MHZ : in TUINT32;
pU32_INIT_STATE_DURATION_US : in TUINT32) is
LU32_COMPARE0 : TUINT32;
-- RTICOMP0
-- UndCC_Begin(All-CallResult), Ignore for this context.
-- UndCC_Begin(All-IdentifierNoOverload)
LS_RTICOMP0 : TS_RTICOMP0;
for LS_RTICOMP0'Address use To_Address(K_RTI_BASE_ADDR + 16#50#);
-- RTITBCTRL
LS_RTITBCTRL : TS_RTITBCTRL;
for LS_RTITBCTRL'Address use To_Address(K_RTI_BASE_ADDR + 16#04#);
-- RTICPUC0
LS_RTICPUC0 : TS_RTICPUC0;
for LS_RTICPUC0'Address use To_Address(K_RTI_BASE_ADDR + 16#18#);
-- RTISETINTENA
LS_RTISETINTENA: TS_RTISETINTENA;
for LS_RTISETINTENA'Address use To_Address(K_RTI_BASE_ADDR + 16#80#);
-- RTIGCTRL
LS_RTIGCTRL : TS_RTIGCTRL;
for LS_RTIGCTRL'Address use To_Address(K_RTI_BASE_ADDR + 16#00#);
-- RTIINTFLAG
LS_RTIINTFLAG : TS_RTIINTFLAG;
for LS_RTIINTFLAG'Address use To_Address(K_RTI_BASE_ADDR + 16#88#);
-- UndCC_End(All-CallResult), Ignore for this context.
-- UndCC_End(All-IdentifierNoOverload)
begin
------------------------------------------------------------------------------
-- *** RTI Timebase Control ***
------------------------------------------------------------------------------
-- Free running Counter 0 (RTIFRC0) clocked by the internal up counter 0 (RTIUC0)
LS_RTITBCTRL.TBEXT := 16#0#;
------------------------------------------------------------------------------
-- *** RTI Compare Up Counter 0 ***
-- The compare up counter 0 register holds the value to be compared with prescale counter 0 (RTIUC0).
-- When the compare shows a match, the free running counter 0 (RTIFRC0) is incremented
------------------------------------------------------------------------------
LS_RTICPUC0.CPUC0 := K_COUNTER_BLOCK_0_PRESCALER - 1;
-- Write the RTI Compare 0 (RTICOMP0) value to generate an interrupt after TIME_INIT
LU32_COMPARE0 := pU32_RTI_FREQ_MHZ*pU32_INIT_STATE_DURATION_US;
-- UndCC_NextLine(All-Division). Division by zero impossible here.
LU32_COMPARE0 := LU32_COMPARE0/(K_COUNTER_BLOCK_0_PRESCALER);
LS_RTICOMP0.COMP0 := LU32_COMPARE0;
------------------------------------------------------------------------------
-- *** RTI Global Control ***
------------------------------------------------------------------------------
LS_RTIGCTRL.CNT0EN := 16#1#; -- Counter 0 enabled
-- Clear INT0-2 flags
LS_RTIINTFLAG.INT0 := 16#1#;
LS_RTIINTFLAG.INT1 := 16#1#;
LS_RTIINTFLAG.INT2 := 16#1#;
------------------------------------------------------------------------------
-- *** RTI Set Interrupt Enable ***
------------------------------------------------------------------------------
LS_RTISETINTENA.SETINT0 := 16#1#; -- Enables Compare Interrupt 0
LS_RTISETINTENA.SETINT1 := 16#1#; -- Enables Compare Interrupt 1
LS_RTISETINTENA.SETINT2 := 16#1#; -- Enables Compare Interrupt 2
-- Enable interrupts for channels 2, 3, 4 and 9 (RTI Compare0, RTI Compare1, RTI Compare2 and GIO high-level)
LS_REQENASET0.REQENASET0 := 16#21C#;
end MARTM_INI_RTI_INIT;
end MARTM_INI_RTI_INIT_PK;