Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TM4C123GH6PM: Problem with debugging

Part Number: TM4C123GH6PM
Other Parts Discussed in Thread: EK-TM4C123GXL

Tool/software: Code Composer Studio

Hello everyone. I'm trying to create three PWM waves in CCS. Initially, the PWM wave is with 20% duty cycle; then when pressing and releasing SW1 it has to turn to 40% and when doing the same with SW2 it should turn to 80%. The "main.c" file compiles but in the debugging section it shows me "Error: Unable to read". What may be wrong with my code? All help Will be welcome.

PD: Some comments and functions are in Spanish language (I'm from Peru)

#include <stdint.h>
#include "tm4c123gh6pm.h"

#define SYS_CTRL_RCC     (*((volatile unsigned long*)0x400FE060))
#define SYS_CTRL_RCGC0     (*((volatile unsigned long*)0x400FE100))
#define SYS_CTRL_RCGC2     (*((volatile unsigned long*)0x400FE108))
#define SYS_CTRL_RCGCADC    (*((volatile unsigned long*)0x400FE638))
#define SYS_CTRL_PRGPIO     (*((volatile unsigned long*)0x400FEA08))
#define SYS_CTRL_RCGCGPIO    (*((volatile unsigned long*)0x400FE608))
#define SYS_CTRL_GPIOHBCTL    (*((volatile unsigned long*)0x400FE06C))

//************************************************************************************************
//-------------------------GPIO PORTB REGISTERS---------------------------------------------------
//************************************************************************************************
#define GPIO_PORTB_DATA    (*((volatile unsigned long*)0x400053FC))
#define GPIO_PORTB_DIR    (*((volatile unsigned long*)0x40005400))
#define GPIO_PORTB_DEN    (*((volatile unsigned long*)0x4000551C))
#define GPIO_PORTB_AFSEL   (*((volatile unsigned long*)0x40005420))
#define GPIO_PORTB_PCTL       (*((volatile unsigned long*)0x4000552C))
#define GPIO_PORTB_AMSEL   (*((volatile unsigned long*)0x40005528))
#define SYS_CTRL_RCGC2_GPIOB  0x00000002

//************************************************************************************************
//-------------------------GPIO PORTF REGISTERS---------------------------------------------------
//************************************************************************************************
#define GPIO_PORTF_DATA    (*((volatile unsigned long*)0x400253FC))
#define GPIO_PORTF_DIR    (*((volatile unsigned long*)0x40025400))
#define GPIO_PORTF_DEN    (*((volatile unsigned long*)0x4002551C))
#define GPIO_PORTF_AFSEL   (*((volatile unsigned long*)0x40025420))

//************************************************************************************************
//-------------------------GPIO PORTE REGISTERS---------------------------------------------------
//************************************************************************************************
#define GPIO_PORTE_DATA    (*((volatile unsigned long*)0x400243FC))
#define GPIO_PORTE_DIR    (*((volatile unsigned long*)0x40024400))
#define GPIO_PORTE_DEN    (*((volatile unsigned long*)0x4002451C))
#define GPIO_PORTE_AFSEL   (*((volatile unsigned long*)0x40024420))
#define GPIO_PORTE_AMSEL   (*((volatile unsigned long*)0x40024528))

//*************************************************************************************************
//------------------------PWM REGISTER-------------------------------------------------------------
//*************************************************************************************************
#define PWM_CTL_R              (*((volatile unsigned long *)0x40028000))
#define PWM_SYNC_R              (*((volatile unsigned long *)0x40028004))
#define PWM_ENABLE_R            (*((volatile unsigned long *)0x40028008))
#define PWM_INVERT_R            (*((volatile unsigned long *)0x4002800C))
#define PWM_FAULT_R             (*((volatile unsigned long *)0x40028010))
#define PWM_INTEN_R             (*((volatile unsigned long *)0x40028014))
#define PWM_RIS_R              (*((volatile unsigned long *)0x40028018))
#define PWM_MISC_R              (*((volatile unsigned long *)0x4002801C))
#define PWM_STATUS_R            (*((volatile unsigned long *)0x40028020))
#define PWM_FAULTVAL_R          (*((volatile unsigned long *)0x40028024))
#define PWM_ENUPD_R             (*((volatile unsigned long *)0x40028028))
#define PWM0_CTL_R              (*((volatile unsigned long *)0x40028040))
#define PWM0_INTEN_R            (*((volatile unsigned long *)0x40028044))
#define PWM0_RIS_R              (*((volatile unsigned long *)0x40028048))
#define PWM0_ISC_R              (*((volatile unsigned long *)0x4002804C))
#define PWM0_LOAD_R             (*((volatile unsigned long *)0x40028050))
#define PWM0_COUNT_R            (*((volatile unsigned long *)0x40028054))
#define PWM0_CMPA_R             (*((volatile unsigned long *)0x40028058))
#define PWM0_CMPB_R             (*((volatile unsigned long *)0x4002805C))
#define PWM0_GENA_R             (*((volatile unsigned long *)0x40028060))
#define PWM0_GENB_R             (*((volatile unsigned long *)0x40028064))
#define PWM0_DBCTL_R            (*((volatile unsigned long *)0x40028068))
#define PWM0_DBRISE_R           (*((volatile unsigned long *)0x4002806C))
#define PWM0_DBFALL_R           (*((volatile unsigned long *)0x40028070))
#define PWM0_FLTSRC0_R          (*((volatile unsigned long *)0x40028074))
#define PWM0_FLTSRC1_R          (*((volatile unsigned long *)0x40028078))
#define PWM0_MINFLTPER_R        (*((volatile unsigned long *)0x4002807C))

//*************************************************************************************************
//------------------------ADC REGISTER-------------------------------------------------------------
//*************************************************************************************************
#define ADC_ACTSS_R             (*((volatile unsigned long *)0x40038000))
#define ADC0_RIS_R              (*((volatile unsigned long *)0x40038004))
#define ADC0_IM_R               (*((volatile unsigned long *)0x40038008))
#define ADC0_ISC_R              (*((volatile unsigned long *)0x4003800C))
#define ADC0_EMUX_R             (*((volatile unsigned long *)0x40038014))
#define ADC0_SSPRI_R            (*((volatile unsigned long *)0x40038020))
#define ADC0_PSSI_R             (*((volatile unsigned long *)0x40038028))
#define ADC0_SSMUX3_R           (*((volatile unsigned long *)0x400380A0))
#define ADC0_SSCTL3_R           (*((volatile unsigned long *)0x400380A4))
#define ADC0_SSFIFO3_R          (*((volatile unsigned long *)0x40038048))
#define ADC_ACTSS_ASEN3         0x00000008  // ADC SS3 Enable
#define ADC_RIS_INR3            0x00000008  // SS3 Raw Interrupt Status
#define ADC_IM_MASK3            0x00000008  // SS3 Interrupt Mask
#define ADC_ISC_IN3             0x00000008  // SS3 Interrupt Status and Clear
#define ADC_EMUX_EM3_M          0x0000F000  // SS3 Trigger Select mask
#define ADC_EMUX_EM3_TIMER      0x00005000  // Timer
#define ADC_SSPRI_SS3_4TH       0x00003000  // fourth priority
#define ADC_SSPRI_SS2_3RD       0x00000200  // third priority
#define ADC_SSPRI_SS1_2ND       0x00000010  // second priority
#define ADC_SSPRI_SS0_1ST       0x00000000  // first priority
#define ADC_PSSI_SS3            0x00000008  // SS3 Initiate
#define ADC_SSMUX3_MUX0_M       0x00000003  // 1st Sample Input Select mask
#define ADC_SSMUX3_MUX0_S       0           // 1st Sample Input Select lshift
#define ADC_SSCTL3_TS0          0x00000008  // 1st Sample Temp Sensor Select
#define ADC_SSCTL3_IE0          0x00000004  // 1st Sample Interrupt Enable
#define ADC_SSCTL3_END0         0x00000002  // 1st Sample is End of Sequence
#define ADC_SSCTL3_D0           0x00000001  // 1st Sample Diff Input Select
#define ADC_SSFIFO3_DATA_M      0x000003FF  // Conversion Result Data mask
//*************************************************************************************************

#define NVIC_EN0_INT19          0x00080000  // Interrupt 19 enable
#define NVIC_EN0_R              (*((volatile unsigned long *)0xE000E100))  // IRQ 0 to 31 Set Enable Register
#define NVIC_PRI4_R             (*((volatile unsigned long *)0xE000E410))  // IRQ 16 to 19 Priority Register
#define TIMER0_CFG_R            (*((volatile unsigned long *)0x40030000))
#define TIMER0_TAMR_R           (*((volatile unsigned long *)0x40030004))
#define TIMER0_CTL_R            (*((volatile unsigned long *)0x4003000C))
#define TIMER0_IMR_R            (*((volatile unsigned long *)0x40030018))
#define TIMER0_MIS_R            (*((volatile unsigned long *)0x40030020))
#define TIMER0_RIS_R            (*((volatile unsigned long *)0x4003001C))
#define TIMER0_ICR_R            (*((volatile unsigned long *)0x40030024))
#define TIMER0_TAILR_R          (*((volatile unsigned long *)0x40030028))
#define TIMER0_TAMR_R            (*((volatile unsigned long *)0x40030004))
#define TIMER0_TAPR_R           (*((volatile unsigned long *)0x40030038))
#define TIMER0_TAR_R            (*((volatile unsigned long *)0x40030048))
#define TIMER_CFG_16_BIT        0x00000004  // 16-bit timer configuration,
                                            // function is controlled by bits
                                            // 1:0 of GPTMTAMR and GPTMTBMR
#define TIMER_TAMR_TAMR_PERIOD  0x00000002  // Periodic Timer mode
#define TIMER_CTL_TAEN          0x00000001  // GPTM TimerA Enable
#define TIMER_IMR_TATOIM        0x00000001  // GPTM TimerA Time-Out Interrupt
                                            // Mask
#define TIMER_ICR_TATOCINT      0x00000001  // GPTM TimerA Time-Out Raw
                                            // Interrupt
#define TIMER_TAILR_TAILRL_M    0x0000FFFF  // GPTM TimerA Interval Load
                                            // Register Low
#define SYSCTL_RCGC1_R          (*((volatile unsigned long *)0x400FE104))
#define SYSCTL_RCGC1_TIMER0     0x00010000  // timer 0 Clock Gating Control
#define SYS_CTRL_RCGC2_GPIOF 0x00000020



//****************************************************************************************************
//--------------RUN MODE CLOCK CONFIGURATION REGISTER (RCC) BITS DEFINITION---------------------------
//****************************************************************************************************
#define   ACG      0x08000000;//Automatic Clock Gating Bit,
#define   SYS_DIV     0x07800000;//Clock Divisor.As we are using PLL so MINSYSDIV used as SYS_DIV
#define   USESYSDIV    0x00400000;//System Clock Divider
#define   USEPWMDIV    0x00100000;//Divsion of clock on PWM clock source.
#define   PWMDIV     0x000E0000;//PWM Frequency Division.
#define   PWRDN     0x00002000;//Clock in POWER DOWN .
#define   BYPASS     0x00000800;//PLL BYPASS bit.
#define   XTAL     0x000007C0;//Crystal Oscillator value.
#define   OSCSRC     0x00000030;//Oscillator Source Bit.
#define   MOSCDIS     0x00000001;//Main Oscillator Disable Bit.

#define   ADC_MODE0    0x00000001;
#define   ADC_MODE1    0x00000002;

#define TM4C123_SW1             1<<4 // Conectado a PF4
#define TM4C123_SW2             1<<0 // Conectado a PF0

#define TWAIT 400000
#define TON   800000

void Pin_PB6_Config(void); //PB6 M0PWM0 inicialización de pines
void PWM0_EstadoInicial(void);
void config_SW1_TM4C123(void);
void config_SW2_TM4C123(void);

uint8_t lectura_sw1_tm4c123(void);
uint8_t lectura_sw2_tm4c123(void);

void PWM0_EstadoSW1(void);
void PWM0_EstadoSW2(void);
//**************************************************************************************************
//Global Flags
//**************************************************************************************************


void main(void){

    void config_pines();

    while(1){
        if(lectura_sw1_tm4c123()){
            PWM0_EstadoSW1(); // si SW1 se pulsa, la onda PWM sera de 40% DC
            while(1){
                if(lectura_sw2_tm4c123()){
                    PWM0_EstadoSW2(); // si SW2 se pulsa, la onda PWM sera de 80% DC
                    break;
                }
            }
        }
    }
}

void config_pines(void){
    config_SW1_TM4C123();
    config_SW2_TM4C123();
	Pin_PB6_Config();
}

void Pin_PB6_Config(void){ //configuración pin PB6
 SYS_CTRL_RCGC0|=0x00100000;//Enable PWM Clock
 SYS_CTRL_PRGPIO|=(SYS_CTRL_RCGC2_GPIOB);//Enable Clock to PORTB
 SYS_CTRL_RCGC2|=(SYS_CTRL_RCGC2_GPIOB);//Enable Clock to PORTB
 GPIO_PORTB_AFSEL|=(0x00000040);//Enable Alternate Function on PB6
 GPIO_PORTB_PCTL&=~0x0F000000;//PORT MUX CONTROL 6
 GPIO_PORTB_PCTL|=0x04000000;//PORT MUX CONTROL 6
 GPIO_PORTB_AMSEL&=~0x40;//Disable Analogue Functionality
 SYS_CTRL_RCC|=0x00100000|(SYS_CTRL_RCC &(~0x000E0000));//Use PWMDIV, DIV_2, BYPASS=0,
 GPIO_PORTB_DIR|=0x0000000F;//Make Output
 GPIO_PORTB_DEN|=0x000000FF;// Digital Data is Enabled
}

void PWM0_EstadoInicial(void){ //definimos PWM con 20% DC (inicial)
   // void config_timer_default(void){ // Configuración Timer 20% DC
        SYSCTL_RCGC1_R |= SYSCTL_RCGC1_TIMER0; // activamos reloj del TIMER0
        // SYSCTL_RCGCTIMER_R |= (1<<0); // activamos reloj del TIMER0
        while(!(SYSCTL_PRTIMER_R & SYSCTL_PRTIMER_R0));//{
        //SYSCTL_PRTIMER_R |= SYSCTL_PRTIMER_R0; // ponemos a 1 el bit correspondiente al registro (para TIMER0 es R0)
        //}

        TIMER0_CTL_R &= ~(1<<0); //deshabilitar timer A
        TIMER0_CFG_R = (TIMER0_CFG_R & ~0x07) + 0x04; // modo 16 bits
        TIMER0_TAMR_R = (TIMER0_TAMR_R & ~0xFFF) + 0x50A; // configuración timer A
        TIMER0_CTL_R |= (1<<6); // TAPWML = 0
        TIMER0_TAILR_R = (TIMER0_TAILR_R & ~(0xFFFF))|39;
        TIMER0_TAPR_R = (TIMER0_TAPR_R & ~0xFF);
        TIMER0_TAMATCHR_R = (TIMER0_TAMATCHR_R & ~(0xFFFF))|19;
        //TIMER0_TAPMR_R =(TIMER0_TAPMR_R & ~0xFF);
 }

void PWM0_EstadoSW1(void){ //definimos PWM con 40% DC (SW1)
    //void config_timer_default(void){ // Configuración Timer 20% DC
        SYSCTL_RCGC1_R |= SYSCTL_RCGC1_TIMER0; // activamos reloj del TIMER0
        // SYSCTL_RCGCTIMER_R |= (1<<0); // activamos reloj del TIMER0
        while(!(SYSCTL_PRTIMER_R & SYSCTL_PRTIMER_R0)); // ponemos a 1 el bit correspondiente al registro (para TIMER0 es R0)

        TIMER0_CTL_R &= ~(1<<0); //deshabilitar timer A
        TIMER0_CFG_R = (TIMER0_CFG_R & ~0x07) + 0x04; // modo 16 bits
        TIMER0_TAMR_R = (TIMER0_TAMR_R & ~0xFFF) + 0x50A; // configuración timer A
        TIMER0_CTL_R |= (1<<6); // TAPWML = 0
        TIMER0_TAILR_R = (TIMER0_TAILR_R & ~(0xFFFF))|59;
        TIMER0_TAPR_R = (TIMER0_TAPR_R & ~0xFF);
        TIMER0_TAMATCHR_R = (TIMER0_TAMATCHR_R & ~(0xFFFF))|39;
        //TIMER0_TAPMR_R =(TIMER0_TAPMR_R & ~0xFF);
}

void PWM0_EstadoSW2(void){ //definimos PWM con 80% DC (SW2)
    //void config_timer_default(void){ // Configuración Timer 20% DC
        SYSCTL_RCGC1_R |= SYSCTL_RCGC1_TIMER0; // activamos reloj del TIMER0
        // SYSCTL_RCGCTIMER_R |= (1<<0); // activamos reloj del TIMER0
        while(!(SYSCTL_PRTIMER_R & SYSCTL_PRTIMER_R0)); // ponemos a 1 el bit correspondiente al registro (para TIMER0 es R0)

        TIMER0_CTL_R &= ~(1<<0); //deshabilitar timer A
        TIMER0_CFG_R = (TIMER0_CFG_R & ~0x07) + 0x04; // modo 16 bits
        TIMER0_TAMR_R = (TIMER0_TAMR_R &~0xFFF) + 0x50A; // configuración timer A
        TIMER0_CTL_R |= (1<<6); // TAPWML = 0
        TIMER0_TAILR_R = (TIMER0_TAILR_R & ~(0xFFFF))|99;
        TIMER0_TAPR_R = (TIMER0_TAPR_R & ~0xFF);
        TIMER0_TAMATCHR_R = (TIMER0_TAMATCHR_R & ~(0xFFFF))|79;
        TIMER0_TAPMR_R =(TIMER0_TAPMR_R & ~0xFF);
}

void config_SW1_TM4C123(void){
    SYSCTL_RCGCGPIO_R |= SYSCTL_RCGCGPIO_R5;
    asm("    nop");
    asm("    nop");
    asm("    nop");
    while(!(SYSCTL_PRGPIO_R & SYSCTL_PRGPIO_R5));

    GPIO_PORTF_DIR_R &= ~(TM4C123_SW1);
    GPIO_PORTF_PUR_R |=  (TM4C123_SW1);
    GPIO_PORTF_DEN_R |=  (TM4C123_SW1);
    GPIO_PORTF_PCTL_R &= ~(0x0F);
    GPIO_PORTF_PCTL_R |= 0x07;
}

void config_SW2_TM4C123(void){
    SYSCTL_RCGCGPIO_R |= SYSCTL_RCGCGPIO_R5;
    asm("    nop");
    asm("    nop");
    asm("    nop");
    while(!(SYSCTL_PRGPIO_R & SYSCTL_PRGPIO_R5));

    GPIO_PORTF_DIR_R   &= ~(TM4C123_SW2);
    GPIO_PORTF_LOCK_R   = 0x4C4F434B;
    GPIO_PORTF_CR_R    |= 0x01;
    GPIO_PORTF_AFSEL_R &= ~(TM4C123_SW2);
    GPIO_PORTF_PUR_R   |=  (TM4C123_SW2);
    GPIO_PORTF_DEN_R   |=  (TM4C123_SW2);
    GPIO_PORTF_PCTL_R &= ~(0x0F);
    GPIO_PORTF_PCTL_R |= 0x07;
}

uint8_t lectura_sw1_tm4c123(void){
    int contador = 0;
    if(!(GPIO_PORTF_DATA_R & TM4C123_SW1)){
        for(contador = 0;contador<TWAIT;contador++);
        while(!(GPIO_PORTF_DATA_R & TM4C123_SW1));
        for(contador = 0;contador<TWAIT;contador++);
        return 1;
    }
    return 0;
}

uint8_t lectura_sw2_tm4c123(void){
    int contador = 0;
    if(!(GPIO_PORTF_DATA_R & TM4C123_SW2)){
        for(contador = 0;contador<TWAIT;contador++);
        while(!(GPIO_PORTF_DATA_R & TM4C123_SW2));
        for(contador = 0;contador<TWAIT;contador++);
        return 1;
    }
    return 0;
}

  • First, we strongly recommend that you not program by writing to each register. Rather that you use the functions in the TivaWare library to setup the GPIO, Timers and other things. Using the proven library functions will simplify your code and greatly reduce the chance of errors. It will also make it easier for people on the forum to help you.

    I don't understand at which point you are getting the "unable to read error". After you program your code into the device, does it successfully get to the beginning of main(), or are you getting an error when trying to program the device?
  • I'm getting an error when trying to program the device in the debug part (it doesn't recognize any register).
  • OK, can you tell me what hardware you are using? Is it the EK-TM4C123GXL launchpad, a custom board or something else? If not the launchpad, what type of JTAG scan controller are you using?
  • I have not heard back from you so I assume you have resolved this issue. If not, please just reply to this thread or open a new thread using "Ask a related question" and I will continue to try and help.