Part Number: TM4C1294NCPDT
Hi,
I have a problem with the SPI speed of my TM4C1294 Launchpad, to which I connected an LCD via SPI.
Effectively I only get an SPI speed of 1.2 MHz, which is too slow for the LCD, which is capable up to 15 MHz SPI speed.
If I specify a higher bitrate in the configuration, no SPI transmission works anymore.
Here is the initialization code:
g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
SYSCTL_OSC_MAIN |
SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_480), 120000000);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOE);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOG);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOH);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOJ);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOK);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOL);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOM);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOP);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOQ);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOR);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOS);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOT);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0);
MAP_SSIDisable(SSI0_BASE); // disables th SSI module as required for init
// Configure the GPIO Pin Mux for PA2
// for SSI0CLK
//
MAP_GPIOPinConfigure(GPIO_PA2_SSI0CLK);
// Configure the GPIO Pin Mux for PA4
// for SSI0XDAT0
//
MAP_GPIOPinConfigure(GPIO_PA4_SSI0XDAT0);
// Configure the GPIO Pin Mux for PA5
// for SSI0XDAT1
//
MAP_GPIOPinConfigure(GPIO_PA5_SSI0XDAT1);
//MAP_GPIOPinConfigure(GPIO_PA3_SSI0FSS);
MAP_GPIOPinTypeSSI(GPIO_PORTA_BASE, GPIO_PIN_4 | GPIO_PIN_5 | GPIO_PIN_2);
/* SOFTWARE CS */
while(!MAP_SysCtlPeripheralReady(SYSCTL_PERIPH_SSI0)){}
MAP_SSIClockSourceSet(SSI0_BASE, SSI_CLOCK_SYSTEM); // sets the system clock as the source of clock
MAP_SSIConfigSetExpClk(SSI0_BASE, MAP_SysCtlClockGet(), SSI_FRF_MOTO_MODE_0, SSI_MODE_MASTER, 1200000, 8);
MAP_SSIAdvModeSet(SSI0_BASE, SSI_ADV_MODE_READ_WRITE);
MAP_SSIEnable(SSI0_BASE); // enables SSI
// LCD_CS
// Configure the GPIO Pin Mux for PA3
// for GPIO_PH0
//
MAP_GPIOPinTypeGPIOOutput(GPIO_PORTA_BASE, GPIO_PIN_3);
//MAP_GPIOPadConfigSet(GPIO_PORTA_BASE, GPIO_PIN_2, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
MAP_GPIOPinWrite(GPIO_PORTA_BASE, GPIO_PIN_3, GPIO_PIN_3);
// LCD_DC
// Configure the GPIO Pin Mux for PD0
// for GPIO_PL1
//
MAP_GPIOPinTypeGPIOOutput(GPIO_PORTP_BASE, GPIO_PIN_1);
//MAP_GPIOPadConfigSet(GPIO_PORTP_BASE, GPIO_PIN_0, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
MAP_GPIOPinWrite(GPIO_PORTP_BASE, GPIO_PIN_1, GPIO_PIN_1);
// LCD_RST
// Configure the GPIO Pin Mux for PD1
// for GPIO_PL0
//
MAP_GPIOPinTypeGPIOOutput(GPIO_PORTG_BASE, GPIO_PIN_1);
//MAP_GPIOPadConfigSet(GPIO_PORTG_BASE, GPIO_PIN_1, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
MAP_GPIOPinWrite(GPIO_PORTG_BASE, GPIO_PIN_1, GPIO_PIN_1);
If I change the initialization code so that I explicitly enter 120 MHz System Clock Speed in MAP_SSIConfigSetExpClk and 30 MHz SPI bitrate, then only 1.2 MHz SPI speed on the LCD gets effective.
MAP_SSIConfigSetExpClk(SSI0_BASE, 120000000, SSI_FRF_MOTO_MODE_0, SSI_MODE_MASTER, 30000000, 8);
In addition, the SPI transmission with real 30 MHz on the LCD should not work at all.
Where could a bug be from me or a bug in the driver library or hardware?