Part Number: TMS570LS3137
Hello ,
Software Reset : writing a 1 to bit 15 of System Exception Control Register (SYSECR) is resetting the processor but the SFR's are retaining the values I want the SFR's to go to Power ON reset values .
While Running TMS570LS3137 firmware in with 4 different project Switching from one project to another in same FLASH area with totally different run requirements .
So if I have to branch from FIXED decision maker to Application , I need to reset all SFR settings that FIXED DECISION MAKER has put in with the values .
FIXED DECISION MAKER address 0x00000000 to 0x00007FFF
UPGRADEBLE APPLICATION address 0x00020000 to 0x000FFFFF
BOOTLODAER APPLICATION address 0x00100000 to 0x0011FFFF
UPGRADEBLE DECISION MAKER add 0x00120000 to 0x0015FFFF