Part Number: TM4C1230E6PM
Other Parts Discussed in Thread: INA219,
Hello,
In my design I used TM4C1230E6PM as controller and INA219 as current shunt amplifier. we faced a weird problem in I2C interface. Also I used 4.7K Ohms pull up resistor for SDA and SCL lines but the problem is we have a drop in SDA line instead of having 0-3.3V pulse it is around between 0-1.8V even I used 1K Ohms resistor but it changed to 0.3V-2.9V. This problem sometimes solved without making any change in design. Also it seems it is occurred randomly but the problem doesn't solve even by changing INA219 or TM4C1230E6PM. If we will not find the problem source we have to change parts for mass production.
Any help would be greatly appreciated.
Sincerely yours,
Siyavash