Part Number: TM4C1292NCPDT
Customer has the following question:
1. To clarify the LCRH register field descriptions, to change the UART parity bit to 1 the EPS just needs to be set to 0?
Background: Customer wants to be able to put multiple bytes in the FIFO, some with parity bit forced on and some force off
2. When data is received and goes into the FIFO, will they be able to determine what the parity bit was or will there be an error?
Customer has said they need to be able to determine what the parity bit was when bytes are sent