This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS570LS3137: shutdown power sequence

Part Number: TMS570LS3137

Tool/software: Code Composer Studio

Hi my name is Chatbot

I use TMS570L3137 as MPU of our products.
I would like to ask about analog input. Vccad is supplied by TPS65381A, while operational amplifier around the analog input of TMS570 is powered by other 5V source (i.e. isolated DCDC converter).
Regarding start-up sequence, at first TPS65381 starts, and the 5V by DCDC starts. So, there is no over current problem for clamp diode of analog input channel.
While in the shutdown sequence, all the power source is cut off at the same time. But there is short difference between TPS65381 and the 5V generated by DCDC. If TPS65381 shutdown before 5V by DCDC by 10m seconds or less, TMS570 gets permanent damage?

Thanks in advance.