Part Number: TM4C1292NCPDT
Tool/software: TI-RTOS
Hi,
Required some help to find the software cause reason
Am trying to making some automation scripts using python, using serial communication
Example :
Command : Turn On Valve, Run Motor @100 RPM
Response : Pass, Motors Runs 100 RPM
When i tried to sending commands individually the script is working fine and logging as well (printing in txt file )
Through automation it is not working it keeps on giving SYSCTL_CAUSE_SW Error. I mean
Just putting all commands in While(1) kind of,
But Exactly am not understanding what was the cause ?
NOTE:- Not Using Watch Dog at well, so there is no chances on Watchdog Reset
Can any one help on this?
Best,
Ugra