Part Number: TM4C1290NCPDT
Other Parts Discussed in Thread: UNIFLASH
Hi All,
Using the boot loader call BL_FLASH_PROGRAM_FN_HOOK, I am able to write the data in 0x20000.
Which I verified by reading it through the memory browser from CCS. Also verified using uniflash with the BIN and the address.
But when I branch or jump using the run command,
(*((void (*)(void))(*(uint32_t *)0x20000)))();
or
((void (*)(void))0x20000)();
the code is not branching to the new application part. Instead I am landing in to fault ISR.
Kindly need support in this issue.
Thanks & Regards,
Yasar Arafath