Part Number: TM4C1294NCPDT
Tool/software: TI C/C++ Compiler
Hi
I'll try to find out whats the difference in some implementations of code - especially the run time.
And my question is what are the comments in the generated assembly files.
LDR A3, [V3, #4] ; [DPU_V7M3_PIPE] |368|
What means the number and why is it jumping around?
Could I see there how long an execution of the code needs out of that?
Kind regards
René
For example in this example out of my code
LDR A3, [V3, #4] ; [DPU_V7M3_PIPE] |368|
UBFX A1, V1, #0, #14 ; [DPU_V7M3_PIPE] |99|
MOV A2, A1 ; [DPU_V7M3_PIPE] |99|
MOV V1, #4270 ; [DPU_V7M3_PIPE] |99|
ADD A4, V3, A2, ASR #2 ; [DPU_V7M3_PIPE] |102|
STRH A2, [V1, +V3] ; [DPU_V7M3_PIPE] |99|
LDRSB A4, [A4, #16] ; [DPU_V7M3_PIPE] |102|
LDR A3, [A3, #1156] ; [DPU_V7M3_PIPE] |368|
SUBS V2, V1, #2 ; [DPU_V7M3_PIPE]
ADDS A2, A2, A4 ; [DPU_V7M3_PIPE] |102|
ADDS A1, A1, A4 ; [DPU_V7M3_PIPE] |102|
SUBS A2, A2, A3 ; [DPU_V7M3_PIPE] |102|
SUBS A1, A1, A3 ; [DPU_V7M3_PIPE] |102|
ASRS A2, A2, #13 ; [DPU_V7M3_PIPE] |102|
LSRS A2, A2, #18 ; [DPU_V7M3_PIPE] |102|
ADDS A3, A1, A2 ; [DPU_V7M3_PIPE] |102|
UXTH A1, A1 ; [DPU_V7M3_PIPE] |102|
AND A3, A3, #49152 ; [DPU_V7M3_PIPE] |102|
ADD A1, A1, A1, LSL #16 ; [DPU_V7M3_PIPE] |102|
PKHBT A2, A3, A2, LSL #16 ; [DPU_V7M3_PIPE] |102|
MOVS A3, #0 ; [DPU_V7M3_PIPE] |115|
USAX A1, A1, A2 ; [DPU_MERLIN_PIPE] |102|
MOVT A3, #0 ; [DPU_V7M3_PIPE] |115|
STR A3, [SP, #0] ; [DPU_V7M3_PIPE] |115|
UXTH A1, A1, ROR #16 ; [DPU_V7M3_PIPE] |102|
STRH A1, [V2, +V3] ; [DPU_V7M3_PIPE] |102|
MOVS A1, #0 ; [DPU_V7M3_PIPE] |117|
MOVT A1, #15540 ; [DPU_V7M3_PIPE] |117|
LDRH A2, [V2, +V3] ; [DPU_V7M3_PIPE] |117|
VMOV S1, A1 ; [DPU_MERLIN_PIPE] |117|
ADD A3, SP, #4 ; [DPU_V7M3_PIPE] |117|