Part Number: RM48L952
Tool/software: Code Composer Studio
Hello,
I am using the freeRTOS and freeRTOS-TCP in a project and would like to enable dynamic stack overflow checking. I am using the TI ARM C/C++ compiler version v18.12.1.LTS.
When I am running the code on the RM48.
if I only add freeRTOS code in my project, i can allocate memory space using function 'pvPortMalloc'.
but after I add freeRTOS and freeRTOS-TCP code,A define 'pvPortMallocSocket' used to allocate the necessary space,By default it also points to the FreeRTOS function 'pvPortMalloc()'
the code doesnt get past prefetchEntry.
In freeRTOS-TCP,The application must be using the heap_4 or heap_5 memory allocator,so I choose the file 'heap_4.c'.
I do not know how to avoid it.
Can you give me some advise?
In freeRTOS,The following code get past prefetchEntry.
In freeRTOS and freeRTOS-TCP,The following code doesnt get past prefetchEntry.