Part Number: TMS570LC4357
Hi,
EMIF_CLK for SDRAM is an output from microcontroller which is enabled when SDRAM CS is asserted.
Can this clock be made free running? Is there any register setting to do so?
Regards,
Archana Rao
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LC4357
Hi,
EMIF_CLK for SDRAM is an output from microcontroller which is enabled when SDRAM CS is asserted.
Can this clock be made free running? Is there any register setting to do so?
Regards,
Archana Rao
Hi Wang,
Thank you for your reply.
During asynchronous memory read/write access, is the internal EMIF_CLK also available on external pin?
We are interfacing this microcontroller with FPGA. Though we are operating in asynchronous mode, we are planning to connect EMIF_CLK to FPGA to avoid metastability at FPGA end.
Regards,
Archana Rao
Hi Archana,
Apologies for late response. The EMIF_CLK is free-running, and you can use this clock for FPGA. The EMIF_CLK is driven from VCLK3. You can configure ECLK to output VCLK3 at test clock mode, and use ECLK for your FPGA.