Part Number: RM48L952
For the EMIF asynchronous interface, is there a defined timing relationship between the EMIF_CLOCK_OUTPUT and the EMIF control signals? I am interfacing to an FPGA and would like to make the memory interface synchronous.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: RM48L952
For the EMIF asynchronous interface, is there a defined timing relationship between the EMIF_CLOCK_OUTPUT and the EMIF control signals? I am interfacing to an FPGA and would like to make the memory interface synchronous.
Thanks you for your quick response. The problem I am having is there is no relationship of the asynchronous bus's chip select, output enable, and read/write signals to any external clock. The microprocessor that is being replaced, defined the relationship between the input clock to the microprocessor and the bus signals. This allowed the FPGA interface to be synchronous to the microprocessor clock. In the RM48 there is no relationship of the bus signals and any external clock which will make the FPGA interface to be totally asynchronous. The design of an asynchronous interface is more complex and this would be a redesign of the currently implemented FPGA interface.
.
John,
The EMIF_CLK signal is a free-running clock and is available as output once enabled. Note that this signal will have a delay through the output buffer in the part, which is not accounted for during the generation of the control signals as specified in the datasheet.
Another possibility is to use the ECLK pin to output a desired clock frequency to the FPGA. The technical reference manual includes information on how to configure ECLK to output different clock domains / sources using the functional clock output mode or the clock test mode.
Hope this helps.
Regards, Sunil