Part Number: TMS570LS3137
Tool/software: TI C/C++ Compiler
Hello Everyone,
I am using HDK(TMS570LS3137). I want to use vsnprintf to write the float values to the result_buffer. Here is the code
#define MAX_BUFFER_SZ (3*1024)
char result_buffer[MAX_BUFFER_SZ];
char * current_ptr=result_buffer;
bool buffer_overflow=false;
int main()
{
printf("Sample %f", 1067.786876f);
return 0;
}
extern "C" int printf(const char * frmt, ...)
{
signed int remaining_bytes= (result_buffer + sizeof(result_buffer))-current_ptr;
signed int num_chars_added = 0;
if (remaining_bytes > 0)
{
va_list vl;
va_start(vl, frmt);
// Print info the output buffer for as many bytes are are left
num_chars_added = vsnprintf(current_ptr, remaining_bytes, frmt, vl);
va_end(vl);
// Did we add characters to the output buffer, if yes then
// advance the current_ptr to the next valid location where the next data
// will be added
if ( num_chars_added > 0)
{
current_ptr = current_ptr + num_chars_added;
}
// vsnprintf returns actual number of bytes that might have been
// copied if the destination buffer was large enough to store the
// string, but the size of the buffer gives was less, a buffer overflow
// condition, so it this happens then set the flag
if( num_chars_added > remaining_bytes)
{
buffer_overflow = true;
}
}
return num_chars_added;
}
I see the float values are not written correctly into the result_buffer.
result_buffer contains : Sample 0.0000000
I am linking library rtsv7R4_T_be_v3D16_eabi.lib. Is there any thing need to be done ?
Thanks