Part Number: EK-TM4C123GXL
Other Parts Discussed in Thread: TM4C123GH6PM
I have been trying to interface 16x2 LCD with TM4C123GH6PM for three days but it didnt work .. the lcd pins VSS VDD VO A K are driven from an outside source (5V)
Here is my Code ..
Thanks in advance .
//*****************************************************************************
#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_memmap.h"
#include "driverlib/debug.h"
#include "driverlib/gpio.h"
#include "driverlib/sysctl.h"
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
while(1);
}
#endif
void LCD_init(void); // LCD_init Prototype
void LCD_Command(uint8_t cmd); // LCD_Command Prototype
void LCD_Data(uint8_t data); // LCD_Data Prototype
int
main(void)
{
volatile uint32_t ui32Loop;
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOD))
{
}
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOB))
{
}
GPIOPinTypeGPIOOutput(GPIO_PORTD_BASE, GPIO_PIN_0);
GPIOPinTypeGPIOOutput(GPIO_PORTD_BASE, GPIO_PIN_1);
GPIOPinTypeGPIOOutput(GPIO_PORTD_BASE, GPIO_PIN_2);
GPIOPinTypeGPIOOutput(GPIO_PORTB_BASE, GPIO_PIN_0);
GPIOPinTypeGPIOOutput(GPIO_PORTB_BASE, GPIO_PIN_1);
GPIOPinTypeGPIOOutput(GPIO_PORTB_BASE, GPIO_PIN_2);
GPIOPinTypeGPIOOutput(GPIO_PORTB_BASE, GPIO_PIN_3);
GPIOPinTypeGPIOOutput(GPIO_PORTB_BASE, GPIO_PIN_4);
GPIOPinTypeGPIOOutput(GPIO_PORTB_BASE, GPIO_PIN_5);
GPIOPinTypeGPIOOutput(GPIO_PORTB_BASE, GPIO_PIN_6);
GPIOPinTypeGPIOOutput(GPIO_PORTB_BASE, GPIO_PIN_7);
GPIOPadConfigSet(GPIO_PORTD_BASE, GPIO_PIN_0, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
GPIOPadConfigSet(GPIO_PORTD_BASE, GPIO_PIN_1, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
GPIOPadConfigSet(GPIO_PORTD_BASE, GPIO_PIN_2, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
GPIOPadConfigSet(GPIO_PORTB_BASE, GPIO_PIN_0, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
GPIOPadConfigSet(GPIO_PORTB_BASE, GPIO_PIN_1, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
GPIOPadConfigSet(GPIO_PORTB_BASE, GPIO_PIN_2, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
GPIOPadConfigSet(GPIO_PORTB_BASE, GPIO_PIN_3, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
GPIOPadConfigSet(GPIO_PORTB_BASE, GPIO_PIN_4, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
GPIOPadConfigSet(GPIO_PORTB_BASE, GPIO_PIN_5, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
GPIOPadConfigSet(GPIO_PORTB_BASE, GPIO_PIN_6, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
GPIOPadConfigSet(GPIO_PORTB_BASE, GPIO_PIN_7, GPIO_STRENGTH_8MA, GPIO_PIN_TYPE_STD);
LCD_init();
LCD_Data('A');
while(1)
{
}
}
void LCD_init(void)
{
uint32_t ui32Loop1;
for(ui32Loop1 = 0; ui32Loop1 < 50000; ui32Loop1++) // 50ms
{
}
LCD_Command(0x3C);
for(ui32Loop1 = 0; ui32Loop1 < 1000; ui32Loop1++) //1 ms
{
}
LCD_Command(0x0F);
for(ui32Loop1 = 0; ui32Loop1 < 1000; ui32Loop1++) //1 ms
{
}
LCD_Command(0x01);
for(ui32Loop1 = 0; ui32Loop1 < 2000; ui32Loop1++) //2ms
{
}
LCD_Command(0x06);
}
void LCD_Command(uint8_t cmd)
{
uint32_t ui32Loop1;
GPIOPinWrite(GPIO_PORTD_BASE, GPIO_PIN_0, 0x0);
GPIOPinWrite(GPIO_PORTD_BASE, GPIO_PIN_1, 0x0);
(*((volatile uint32_t*)(0x400053FC))) = cmd;// write cmd to DATA register in PORT B
GPIOPinWrite(GPIO_PORTD_BASE, GPIO_PIN_2 , GPIO_PIN_2 );
for(ui32Loop1 = 0; ui32Loop1 < 2000; ui32Loop1++)
{
}
GPIOPinWrite(GPIO_PORTD_BASE, GPIO_PIN_2 , 0x0);
}
void LCD_Data(uint8_t data)
{
uint32_t ui32Loop1;
GPIOPinWrite(GPIO_PORTD_BASE, GPIO_PIN_0 , GPIO_PIN_0 ); // rs
GPIOPinWrite(GPIO_PORTD_BASE, GPIO_PIN_1, 0x0); // rw
(*((volatile uint32_t*)(0x400053FC))) = data; // write data to DATA register in PORT B
GPIOPinWrite(GPIO_PORTD_BASE, GPIO_PIN_2 , GPIO_PIN_2); // en
for(ui32Loop1 = 0; ui32Loop1 < 2000; ui32Loop1++)
{
}
GPIOPinWrite(GPIO_PORTD_BASE, GPIO_PIN_2 , 0x0);
}