Part Number: TMDX570LC43HDK
Other Parts Discussed in Thread: HALCOGEN
Dear all, I am currently modifying the SCI loopback DMA example to link the data transfer to a physical button on the dev board. The behaviour is as expected, when i press the button 8 times the exception is triggered as configured in the DMA control packet. The problem comes when I try to real RX_DATA inside the ISR, it is set to all zeroes, but i can see before triggering that the data are actually being written there. I am not an expert on this board/processors, so i might have been missing something or this is not the correct way to retrieve data. I attach my main function code, the project was generated by Halcogen 4.7.1 and developed in CCS Version: 7.4.0.00015
/** @file HL_sys_main.c
* @brief Application main file
* @date 11-Dec-2018
* @version 04.07.01
*
* This file contains an empty main function,
* which can be used for the application.
*/
/*
* Copyright (C) 2009-2018 Texas Instruments Incorporated - www.ti.com
*
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the
* distribution.
*
* Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
* "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
* LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
* A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
* OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
* SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
* LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
* DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
* THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
* (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
* OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*
*/
/* USER CODE BEGIN (0) */
/* USER CODE END */
/* Include Files */
#include "HL_sys_common.h"
/* USER CODE BEGIN (1) */
#include "HL_system.h"
#include "stdio.h"
#include "HL_gio.h"
#include "HL_sci.h"
#include "HL_sys_dma.h"
/* USER CODE END */
/** @fn void main(void)
* @brief Application main function
* @note This function is empty by default.
*
* This function is called after startup.
* The user can use this function to implement the application.
*/
/* USER CODE BEGIN (2) */
#define size 8
/* External connection (SCI3 TX -> SCI4 RX) is needed in case LOOPBACKMODE is defined as 0 */
#define LOOPBACKMODE 1
/* Rx data buffer */
uint8_t RX_DATA[size] = { 0 };
/* Addresses of SCI 8-bit TX/Rx data */
#if ((__little_endian__ == 1) || (__LITTLE_ENDIAN__ == 1))
#define SCI3_TX_ADDR ((uint32_t)(&(sciREG3->TD)))
#define SCI3_RX_ADDR ((uint32_t)(&(sciREG3->RD)))
#define SCI4_TX_ADDR ((uint32_t)(&(sciREG4->TD)))
#define SCI4_RX_ADDR ((uint32_t)(&(sciREG4->RD)))
#else
#define SCI3_TX_ADDR ((uint32_t)(&(sciREG3->TD)) + 3)
#define SCI3_RX_ADDR ((uint32_t)(&(sciREG3->RD)) + 3)
#define SCI4_TX_ADDR ((uint32_t)(&(sciREG4->TD)) + 3)
#define SCI4_RX_ADDR ((uint32_t)(&(sciREG4->RD)) + 3)
#endif
#define DMA_SCI3_TX DMA_REQ31
#define DMA_SCI3_RX DMA_REQ30
#define DMA_SCI4_TX DMA_REQ43
#define DMA_SCI4_RX DMA_REQ42
#define SCI_SET_TX_DMA (1<<16)
#define SCI_SET_RX_DMA (1<<17)
#define SCI_SET_RX_DMA_ALL (1<<18)
/* USER CODE END */
int main(void)
{
/* USER CODE BEGIN (3) */
//uint32 sciTxData, sciRxData;
uint32 sciRxData;
//g_dmaCTRL g_dmaCTRLPKT1, g_dmaCTRLPKT2;
g_dmaCTRL g_dmaCTRLPKT2;
gioInit();
sciInit();
#if LOOPBACKMODE == 1
/* Enable SCI loopback */
sciEnableLoopback(sciREG3, Digital_Lbk);
while (((sciREG3->FLR & SCI_TX_INT) == 0U) || ((sciREG3->FLR & 0x4) == 0x4))
{
} /* Wait */
/*Assign DMA request SCI3 receive to Channel 1*/
dmaReqAssign(DMA_CH1, DMA_SCI3_RX);
sciRxData = SCI3_RX_ADDR;
#else
while (((sciREG3->FLR & SCI_TX_INT) == 0U) || ((sciREG3->FLR & 0x4) == 0x4))
{
} /* Wait */
/*Assign DMA request SCI3 transmit to Channel 0*/
//dmaReqAssign(DMA_CH0, DMA_SCI3_TX);
/*Assign DMA request SCI4 receive to Channel 1*/
dmaReqAssign(DMA_CH1, DMA_SCI4_RX);
sciTxData = SCI3_TX_ADDR;
sciRxData = SCI4_RX_ADDR;
#endif
/*Configure control packet for Channel 1*/
g_dmaCTRLPKT2.SADD = sciRxData; /* source address */
g_dmaCTRLPKT2.DADD = (uint32_t) RX_DATA; /* destination addr ss */
g_dmaCTRLPKT2.CHCTRL = 0; /* channel control */
g_dmaCTRLPKT2.FRCNT = size; /* frame count */
g_dmaCTRLPKT2.ELCNT = 1; /* element count */
g_dmaCTRLPKT2.ELDOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT2.ELSOFFSET = 0; /* element destination offset */
g_dmaCTRLPKT2.FRDOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT2.FRSOFFSET = 0; /* frame destination offset */
g_dmaCTRLPKT2.PORTASGN = PORTB_READ_PORTA_WRITE;
g_dmaCTRLPKT2.RDSIZE = ACCESS_8_BIT; /* read size */
g_dmaCTRLPKT2.WRSIZE = ACCESS_8_BIT; /* write size */
g_dmaCTRLPKT2.TTYPE = FRAME_TRANSFER; /* transfer type */
g_dmaCTRLPKT2.ADDMODERD = ADDR_FIXED; /* address mode read */
g_dmaCTRLPKT2.ADDMODEWR = ADDR_INC1; /* address mode write */
g_dmaCTRLPKT2.AUTOINIT = AUTOINIT_OFF; /* autoinit */
/*Set control packet for channel 0 and 1*/
// dmaSetCtrlPacket(DMA_CH0, g_dmaCTRLPKT1);
dmaSetCtrlPacket(DMA_CH1, g_dmaCTRLPKT2);
/*Set dma channel 0 and 1 to trigger on hardware request*/
// dmaSetChEnable(DMA_CH0, DMA_HW);
dmaSetChEnable(DMA_CH1, DMA_HW);
/*Enable DMA*/
dmaEnable();
dmaEnableInterrupt(DMA_CH1, BTC, DMA_INTA);
/*Enable button for GioA 7*/
gioEnableNotification(gioPORTA, 7);
#if LOOPBACKMODE == 1
/*Enable SCI3 Receive DMA Request*/
sciREG3->SETINT |= SCI_SET_RX_DMA | SCI_SET_RX_DMA_ALL;
#else
/*Enable SCI3 Transmit and SCI4 Receive DMA Request*/
sciREG3->SETINT |= SCI_SET_TX_DMA;
sciREG4->SETINT |= SCI_SET_RX_DMA | SCI_SET_RX_DMA_ALL;
#endif
_enable_IRQ();
while (1)
;
/* USER CODE END */
return 0;
}
/* USER CODE BEGIN (4) */
uint8 buffer[1];
uint8 incrementalT = 'a';
int vecesBoton = 0;
int i = 0;
void gioNotification(gioPORT_t *port, uint32 bit)
{
buffer[0] = incrementalT;
sciSend(sciREG3, 1, buffer);
incrementalT++;
vecesBoton++;
}
int incrementalR = 0;
void dmaGroupANotification(dmaInterrupt_t inttype, uint32 channel)
{
incrementalR++;
dmaSetChEnable(DMA_CH1, DMA_HW);
}
/* USER CODE END */
Best Regards