Part Number: TMS570LS0714
Other Parts Discussed in Thread: HALCOGEN
Hi Team,
My customer face an issue when they are using FEE operation before flash erase one bank, if add flash erase function as below(band 0), and do fee write operation, there will cause watchdog reset, if they remove the flash erase function, then everything is ok without reset. is there any relationship between flash erase operation and fee operation ?
status = Fapi_BlockErase(Bank,Flash_Start_Address,Size_In_Bytes); // if remove this function , then everything is ok.