Part Number: TM4C1294NCPDT
In one of my prototype, after flashing in the codes, the micro gets burning hot when I try to debug it via JTAG, and I try to find out the reason.
In this design, the micro is powered by normal power and backed up by supercaps. When the normal power is removed, the Vcc will be supplied by supercaps and gradually drop from 3.3V to 0 within 10 seconds. If XDS100v3 is connected to the JTAG port of the micro, it may still try to communicate with the micro, so the voltage on JTAG lines are higher than "Vcc" of the micro, would this post a problem to the micro?