Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: ISO1050
Tool/software: Code Composer Studio
Hi Team,
We are planning to use TM4C1294NCPDT in our custom design. Can anyone please confirm the following:
1) Does TM4C1294NCPDT have support to integrate SPI based NOR Flash and QSPI based NOR flash? What is the maximum clock speed that can be supported and doe we have any driver support for SPI/QSPI?
2) Is TM4C1294NCPDT capable of self OTA update from Flash or through CAN/Ethernet/RS485?
3) Is there any reference design for isolated CAN interface using TM4C1294NCPDT?