Part Number: EK-TM4C1294XL
Other Parts Discussed in Thread: LM3S811, , UNIFLASH
Hi,
We have been using the older LM3S811 EVAL Board to program the LM3S series of devices earlier and now to program the TM4C1294 devices on our custom boards.
We use the 10pin JTAG port to program our custom boards.
1. Can we use the EK-TM4C1294XL board to program these devices on our custom boards ?
2. Will the LM FLASH PROGRAMMER and UNIFLASH both work for programming the custom TM4C1294 boards ?
3. Section 2.3.1 of the "spmu365c" document says, "....Debug out of the ICDI is possible by removing resistors R6, R7, R8, R10, R11, R15, R16 and R40 from the Connected Launch Pad and use the ICDI to drive JTAG signals out on U6 for the purpose of programming or debugging other boards....."
So, is that all that we need to do to program our custom TM4C1294 boards ?
4. Can we also program the MAC address on our custom boards as above ?
Thanks
Shashi