Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS3137: TMS570LS3137

Part Number: TMS570LS3137
Other Parts Discussed in Thread: HALCOGEN,

In TMS570LS3137 halcogen generated code, Voltage Monitor reset is not handled. In reference manual details of Voltage Monitor reset are provide much.

Requesting you to provide more details about it.

  • Hello,

    The purpose of this voltage monitor (VMON) is to eliminate the requirement for a specific sequence when powering up the core and I/O voltage supplies. The VMON only monitor VCC and VCCIO. It doesn't monitor VCCAD and VCCP.

    When the voltage monitor detects a low voltage on the I/O supply, or detects an out-of-range voltage on the core supply, it asserts a power-on reset. The voltage monitor is not an alternative for an external voltage supervisor.The external voltage supervisor circuit is recommended to guarantee that the device is held in reset when the voltage supplies are out of range. This feature is not programmable, and the external power supply is also not controllable by the SW.

    TPS75381 is a good part for TMS570 device.