This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UNIFLASH: TI Cloud Agent instalation

Part Number: UNIFLASH
Other Parts Discussed in Thread: IWR1443

Hi,

To utilize Uniflash tool, I want to install Ti Cloud Agent into my PC (32bit-windows7pro, Japanese),

but I cannot do it.

Attached is the error console of installer. Error message in Japanese is following; 

The version of this(these) file(s) is not compatible with those of the current running Windows.

Check system information of your computer and ask software provider which type of program version, x86(32bit) or x64(64bit).

Shall I modify some conf. file(s) before installing?  Please give suggestions.

Thanks,

Kaneko.

  • Kaneko-san,

    katsuyuki kaneko said:
    To utilize Uniflash tool, I want to install Ti Cloud Agent into my PC (32bit-windows7pro, Japanese),

    Windows 32-bit is no longer supported by current tools. To use UniFlash with Windows 32-bit, I recommended UniFlash 4.6 Desktop version:

    http://processors.wiki.ti.com/index.php/CCS_UniFlash_v4.6.0_Release_Notes#Installation_Instructions

    Thank you

    ki 

  • ki-san;

    Thank you for your advice.

    I successfully installed Uniflash v4.6.0 and find it works. (But still not flashing .bin file  due to another problem....)

    Now I have another question.

    After replacing Uniflash (I do not know there is any relations or not), mmWave Demo visualizer (ver.2.1.0) does not work.

    In particular, Demo visualizer requests 'Ti cloud agent download'  when I configure COM port. (not seen before)

    And I try to install Ti cloud agent, during installation, I encounter the same error message regarding windows versions.

    My question is;

    (1) Similar to Uniflash, does Ti cloud agent have x86- compatible/incompatible versions?

    (2) Are there any internal dependency (e.g. internal components or drivers) among Uniflash, Demo visualizer and Ti cloud agent.

    Thanks in advance,

    kaneko.

  • ki-san;

    Thank you for your help.

    I'd like to add one question.

    As Ti recommends web-version of Uniflash in the latest environment, is it possible to use

    previous version (e.g. v.4.6.0) of web-based Uniflash?

    If it's possible, please let me know.

    Thanks,

    kaneko

  • Kaneko-san,

    Unfortunately, all the on-line cloud based tools (UniFlash Cloud and TI Cloud Agent) only support 64-bit OS now. There is no way to revert back to earlier versions that support 32-bit. You will need to stick to older desktop based versions to use it with your 32-bit Windows. And, unfortunately, you will not be able to run the mmWave Demo Visualizer on 32-bit Windows since you need TI Cloud Agent. Sorry.

    Thank you,

    ki

  • Ki-san;

    Thank you for your suggestion.

    I successfully flash IWR1443 device and replace .bin file by using Uniflash v4.6.0.

    Also I will replace my environment into 64-bit windows by your recommendation.

    Thanks,

    Kaneko.