This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS570LC4357: SCI Rx Count Using DMA

Part Number: TMS570LC4357

Tool/software: Code Composer Studio

Hi,

I have set up the SCI3 Rx with DMA, where i am receiving the data correclty.

But, now i need to check the number of frames received after the transmission and want to clear it, so how can i do that.

I want to monitor the dma transfer count and accordingly the data received.

I tried by reading the CFTCOUNT but it is showing the fixed value(which is 0x1F980000)  irrespective of the frame size.

There is a need to check this count and clear the respective bit for starting the counting again for the new coming data.

How can i achieve this?

Can anyone please help me out in this.

Regards,

Shivam Kakad