Part Number: TMS570LC4357
Is there any way to force the MibSPI sequencer to reset or repopulated the transmit shift register without re-initializing the SPI peripheral? I am using a TMS570 as a slave SPI device for asynchronous data transfers. I am using a single TG and 8 buffers with 2 Rx DMAs and 2 Tx DMAs to move half of the tx/rx data each. I am noticing that the fist byte of data that is transmitted on SPI is 1 frame old (i.e. it is the same data DMA'd from RAM at the end of the SPI transfer). I think this is due to the Tx DMA being triggered at the end of the SPI transfer which causes the sequencer to update the tx shift register. However I want to be able to update the tx data periodically if the SPI transfer is complete, but the first byte is always stale on subsequent SPI transfers.