Part Number: TMS570LS1227
Hi,
We've just come across an issue where we do not appear to be allowing sufficient time to erase one of the data flash banks. We haven't seen this particular issue before, even though we've got a fair number of boards\processors that have been in use for, in some cases, years.
The TRM for the 1227 specifies that the erase time for the bank 7 flash is:
| Min | Nom | Max | Unit | |
| -40C to 125C | - | 0.2 | 8 | s |
| 0C to 60C, for first 25 cycles | 14 | 100 | ms |
I guess what we'd like to know is whether there is any more data available for the data flash erase times? Perhaps some graphs or tables that show the effect of time and\or age on the erase times? Especially as there seems to be a large difference between the '0C to 60C, for first 25 cycles' and the '-40 to 125C' timings.
Best regards,
Steve