Other Parts Discussed in Thread: ADS1220, MSP430I2041
in the title. . .
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Greeting & Welcome, (to a first-time poster)
The (primarily) young, female, college students - who so well support my small tech firm - note that (perhaps for 'good reason') 'No such 24-bit LPads or Boosters are to be found here. (or at/by competing site offerings...)
Why then - is that? Twenty-Four bits is a 'Big Deal' and imposes a 'mighty challenge' - delivered across multiple, engineering disciplines. (even pcb design - especially pcb design)
So - w/those 'facts in evidence' - should it not be asked:
You may note that many (perhaps most) of the 'pro firms' who deploy such devices (20/22/24 bits) do so to enhance, 'Dynamic Signal Range' - not just added signal resolution.
It is believed that 16 bits - perhaps even 18 bits - are far more likely to be (somewhere) available - and (they) may prove a superior choice. In addition - your use of a 'ready made/tested' Eval Board (not only a Booster) is much preferred over a 'user attempted - pcb design & layout.' Bread-boards - almost surely - have 'No chance of succeeding' at this level of ADC resolution.
Hi
For MSP430, we have some 24-bit sigma delta devices. You can refer to this http://www.ti.com/microcontrollers/msp430-ultra-low-power-mcus/products.html#~p121=24-bit%20Sigma%20Delta
That is better to provide more information about your project and we will give you a better choice.
Best regards
Gary
Hi Gary! My project is a wheatstone with a desired step resolution of ~25-35uV and a total range of ~8mV.
To resolve that with minimal error, I believe I'd need >18-bits, ENOB. It seems like the TI mcu ecosystem has on-board ADC offerings in (mostly) 16-bits then jumps to 24-bits.
I am not at all familiar with TI products though.
It would be ideal to start with a launchpad, for ease of entry into the IDE. But alternately, I will try a non-launchpad mcu.
Or a separate ADC. The ADS1220 keeps coming across my radar. But I am not sure if this is a great product for this application.
Hi
Take the MSP430I2041 for example. If you use the internal 1.2V reference, that can get a desired resolution of 4.5uV and if consider the error that should meet your need 25uV.
What's more do you need some communication interface? The MSP430 can give more peripherals that you may need and you can do some data processing.
Best regards
Gary