Part Number: TMS570LS1227
Hi Team,
I am using MCAL version AUTOSAR MCAL 05.40.00 EA1 and EB tresos 21.0.0. The target MCU is TMS570L1227
The PWM module cause the system go to error status when running Pwm_Init() function.
Please help to identify the error cause and solve the problem.
My PWM module configuration is as below:
When run to following code, the system will go to OS exception
The Call stack when error happens is as below:
The following pic show the status when the PWM_Init() function is entered