Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: EMIF Self testing

Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN

Hi Team,

I wanted to use the Emif by using Chip Select 2.

For the self testing, I have provided its address(0x60000000) and writing the data at that address.

To check whether it is working i connected the CRO probes to one of the address lines, but i could not able to see anything on it.

I am configuring the CE2CFG register as 0x083441A9 for the emif clk to be operated at 90MHz.

Can anyone please suggest me any method to check the working of the Emif.

Regards,

Shivam Kakad

  • Hello Shivam,

    Please make sure the setup time, strobe time, and hold time meet the requirements defined in datasheets (TMS570 and SRAM datasheet).

    If cache is enabled, please configure the 0x6000_0000 memory MPU region as write-through instead of write-back (MPU tab in HALCoGen).

    If the memory is 16 bit, address 0 of the memory should be connected to EMIF BA[1], and address 1 is connected to EMIF address[0].

  • Hi Wang,

    I have tried the following things:

    #define Chip_Select_2 ((uint32 *)0x60000000U)

    int count= 1;
    uint8* address = Chip_Select_2;
    while(1)
    {
    if(address < 0x63ffffff)
    {
    *address = count;
    count++;
    address++;
    }
    }

    here, I am trying to increment the address value by sending the byte, and i have observed that:

    For,

    Address Line A0: it remain as 1


    Address Line A1: it toggles after 8 bytes are transmitted

                                ie. for address from 0x60000000 - 0x60000007 it remains 0 and after that goes to 1 for next 8 count

    Address Line A2: it toggles after 16 bytes are transmitted

                                i.e. address from 0x60000000 - 0x6000000E it remains 0 and after that 1 for next 16 count

    Address Line A3: it toggles after 24 bytes are transmitted

                                i.e. address from 0x60000000 - 0x60000016 it remains 0 and after that 1 for next 24 count

    and so on...

    is it expectable the same for the Emif? Does my observations are correct?

    Please assist me.

    Regards,

    Shivam Kakad

  • Hello Shivam,

    Let me explain the emif address for you:

    The CS2 EMIF memory address: 0x6000_00XY which X[3:0] and Y[3:0] are 4-bit binary number

    EMIF_A0 -- Y[2]

    EMIF_A1 -- Y[3]

    EMIF_A2 -- X[0]

    EMIF_A3 -- X[1]

    So for emif address 0x6000_005A (XY=01011010b), EMIF_A0=0, EMIF_A1=1, EMIF_A2=1, EMIF_A3=0.

    Address Line A0: it remain as 1 ---> Not correct


    Address Line A1: it toggles after 8 bytes are transmitted ---> correct

                                ie. for address from 0x60000000 - 0x60000007 it remains 0 and after that goes to 1 for next 8 count

    Address Line A2: it toggles after 16 bytes are transmitted -->correct

                                i.e. address from 0x60000000 - 0x6000000E it remains 0 and after that 1 for next 16 count

    Address Line A3: it toggles after 24 bytes are transmitted --> correct

                                i.e. address from 0x60000000 - 0x60000016 it remains 0 and after that 1 for next 24 count

  • Thanks Wang for the detail description.

    Can you please tell me the address mapping for the EMIF.

    How the mapping of this a0 to a21 lines has been done for the chip select 2, and whether that is same for the other chip selects and sdram as well?

    As well as for the data mapping i would be keen to know.

    Please provide the document if any.

    Regards,

    Shivam Kakad

  • Hi Wang,

    As per the description you provided i could not able to get the results.

    for A0 it is continuously staying at 1,

    for A1 it change the status at

    07->0F->17->1F->27->2F->37->3F->...

    for A2 it change the status at

    0F->1F->2F->3F->4F->5F->...

    for A3 it change the status at

    17->37->57->97->B7->...

    for A4 it change the status at

    37->77->B7->...

    Why is it showing such status.

    How the logical and functional mapping is there for the address line?

    Can you please provide me the document for the address mapping of it, so that i can relate to it?

    Thanks in advance.

    Shivam Kakad

  • Hello Shivam,

    Is there a memory attached to EMIF? After you write data to EMIF memory, is the data is correct location of the EMIF memory? Please refer to Interfacing to Asynchronous Memory in EMIF chapter of TRM.

  • Hi Wang,

    No device is connected to EMIF and would like to test EMIF module without connecting any to it. So, help us in testing them and provide us the details as requested by Shivam.

  • As I said, the A0 =1 always is not correct. Please read the EMIF chapter for details.

  • Hi Wang,

    Can you please provide us the complete bit mapping details of address and data lines, so that it will be clearer for us?
    We are seeing A0 to 1 and do you see any reason or anything to be checked further on why it is setting it up?

  • Hello,

    I told you that BA0 is bit 1 of the logic address, A0 is bit 2 of the logic address for 16-bit Async mode. If you write data to the address of 0x6000_0004/8/C, the A0 is 1, other locations the A0 is 0.

    It may be caused by many things: wrong pin is probed, pinmux for A0 is not configured correctly, schematics issue, etc.