Part Number: BOOSTXL-SENSHUB
Tool/software: Code Composer Studio
Helo,
I managed to get the mpu9150 Accel/gyro/mag sensor with the tm4c123 - with the provided sample code. (compdcm_mpu9150). I have simplified the code a bit, taking out led driver, and serial output in order to measure the speed that the data is sampled at from the sensor.
Instead of measuring sample rate programmatically, I have attached a scope to GPIOB PIN 2, and I am able to see the interrupt happening from the sensor, and it looks like 20ms each reading approximately.
I tried to find relevant parts of the code, but I could not find where to adjust the sample rate.
// Write application specific sensor configuration such as filter settings
// and sensor range settings.
g_sMPU9150Inst.pui8Data[0] = MPU9150_CONFIG_DLPF_CFG_94_98;
//g_sMPU9150Inst.pui8Data[0] = MPU9150_CONFIG_DLPF_CFG_184_188;
g_sMPU9150Inst.pui8Data[1] = MPU9150_GYRO_CONFIG_FS_SEL_250;
g_sMPU9150Inst.pui8Data[2] = (MPU9150_ACCEL_CONFIG_ACCEL_HPF_5HZ | MPU9150_ACCEL_CONFIG_AFS_SEL_2G);
I tried to change MPU_CONFIG_DLPF_CFG_94_98 to MPU9150_CONFIG_DLPF_CFG_184_188, as defined at the hw_mpu9150.h file, but that did not had an effect at the sample rate measured by the scope.
Any ideas/recomendations/help greatly appreciated.
Best regards,
Can