Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS570LC4357: Link between CCS and HALCOGEN

Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN

Tool/software: Code Composer Studio

I am starting to learn coding with CCS and HALCOGEN with my new Hercules MCU development KIT.   I made a project based on the tutorial for both CCS and HALCOGEN.   I used HALCOGEN to generate the code.  What I got confused is:   In CCS the project generated a file called main.c in the project root directory.   The code generated by HAL are in /include and /source directories.   Based on the tutorial there should be a file called sys_main.c,  but I can't find that file.   The files generated by HALCOGEN all starts with HL_,   and there is a file called HL_system.c,  but it doesn't have the main{} function call in it.   So what is the main file generated by HALCOGEN,  and how can I link that file to the main.c file generated by CCS?