This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TM4C1294NCPDT: CMSIS- Importing Source folder into the project

Part Number: TM4C1294NCPDT

Tool/software: Code Composer Studio

I am using the CCS version 9.0.1 with the CMSIS DSP library Downloaded from refering this document http://www.ti.com/lit/an/spma041g/spma041g.pdf.

I have followed the exact same steps as entioned in the document. But every time I am getting the following error while importing the Source Folder into the project....Problem encountered while importing the project with the following error detail.

Then also if I continued with pressing Finish its not giving me any error.

Further while configuring all the build properties, In the Advanced option> Assembler option...i am not getting the option for UAL i.e. unified assembly language to tick mark.

After all this when go for building the project it gives me two types of error i.e. 

fatal error: cannot open source file "core_cm4.h in ccs studio

define is missing its parameter 'NAME[=value]'


I have gone through this thread which I have mentioned https://e2e.ti.com/support/microcontrollers/other/f/908/p/390789/1382173

I have included all those definitions in Pre-Defined symbols... Then also I  am getting this types of error.

Please help me out with this so I can move forward