Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN, UNIFLASH
Tool/software: Code Composer Studio
I have problem using ADC block. I am trying to start the ADC module and capture some data from the ADC data memory block. I used HALCOGEN to generate the template and picked some arbitrary channels for ADC groups. I chose channels 0 1 2 3 for group 0, 4 5 6 7 for group one and 8 9 10 11 for group 2. Then I used the following code:
int i;
adcInit();
adcStartConversion(adcREG1, 0); /*Start ADC1 EV Group conversion */
adcStartConversion(adcREG1, 1);
adcStartConversion(adcREG1, 2);
adcStartConversion(adcREG2, 0); /*Start ADC2 Group 1 conversion */
adcStartConversion(adcREG2, 1);
adcStartConversion(adcREG2, 2);
for(i = 0; i<1024; i++){
/*wait for 1024 cycles */
}
adcStopConversion(adcREG1, 0);
adcStopConversion(adcREG1, 1);
adcStopConversion(adcREG1, 2);
adcStopConversion(adcREG2, 0);
adcStopConversion(adcREG2, 1);
adcStopConversion(adcREG2, 2);
After running the code I checked ADC memory block with uniFlash. The data in the block doesn't seem to be written by ADC. In file HL_adc.c, I saw function called adcGetData, do I need to use this function to write data to memory block? The function has an agrument called adcData_t, which I can't find the definition.
Thanks,
XG