Part Number: TM4C1294NCPDT
Hello,
can the port be damage when the GPIO output is high and accidentally is shorten to GND?
Regards, Holger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TM4C1294NCPDT
Hello,
can the port be damage when the GPIO output is high and accidentally is shorten to GND?
Regards, Holger
Outsider ALERT!
Much depends upon:
I'd be wary of 'Space Launch' and/or 'Medical Implantation' - w/that MCU. It should be 'quick/easy' to Toggle that GPIO - after placing a proper resistive load - and observing the resulting waveform. Better still - add the same value load resistor to a GPIO on another Port (in case the pin & (even) port was damaged/impacted) - and toggle both (the 'accident') and your 'normal' GPIO - looking for differences. Higher frequency toggle rates may prove best at revealing damage.
It would be wise to measure the MCU's current draw - both @ idle and while toggling both (ports & pins). A 2nd MCU should be subjected to the same exercise - and results compared...
Note too that 'some' report should have emerged - from the person who recognized/discovered the illegal connection. Was the MCU 'hot' - or otherwise stressed? (i.e. test code stuttered or otherwise failed) These are 'pretty strong little beasts' - and often will survive - such abuse... (especially when the 'offending current source' is the pin itself - no such 'survival' is likely - when an unlimited current arrives from an external source!)
For the most demanding, critical & robust of applications - it proves 'SOP' to install current-limiting (protecting) resistors (usually a resistive network) upon each/every (especially external signal receiving) MCU GPIO pin(s)...