This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357: EMIF_nDQM[0] no in input multiplexing table

Part Number: TMS570LC4357

Hello,

Please refer to page 37 of the tms570lc4357 Datasheet, there it states that EMIF_nDQM[0] can be on ball E10 or B13. Then at the bottom of the table it says that the ball can be chosen as the input multiplexing table indicates , but in the input multiplexing table EMIF_nDQM[0 does not appear (same for DQM[1] and other EMIF signals). Is it possible that in a new device the DQM0 signal is by default in B13? How can I change or make sure that it is in E10?

Best wishes

Tony