This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS570LC4357: L2RAMW module Error Status Register RAMERRSTATUS field description

Part Number: TMS570LC4357

Tool/software: Code Composer Studio

When I read the TMS570LC4357 spun563a manual I am kind of confused.   In table 8-4 it says in the field of RAMERRSTATUS normally a 1 represents an error detected and 0 means no error detected.  However it also says "This bit must be cleared by writing a 1 to it before any new error can be generated.".   If 1 means error detected,  won't the bit be reset to 0 to detect future error?  Is this a typo or I understand wrong?

Thanks,

XG