Part Number: TM4C123GH6PM
请问,我用ccs6.2 配置的TM4C123GH6PM工程,我想设置ccs使得我写代码时 ,再输入几个字符后,会提示匹配 需要怎么配置呢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TM4C123GH6PM
请问,我用ccs6.2 配置的TM4C123GH6PM工程,我想设置ccs使得我写代码时 ,再输入几个字符后,会提示匹配 需要怎么配置呢。
Thank you - now (maybe/hopefully) it is possible for 'native English speakers' to assist.
If you are asking, "Which of these 3 methods proves best for your specific use" - then the answer becomes, 'It depends.'
These 'optimization levels' usually center upon 'MCU Execution Speed' and/or 'MCU Code Size.' And - such choice is made by the user - on a 'Case by Case Basis.' Usually one finds it difficult to optimize (both) Speed & Code Size. And helpfully - most usually (only one) of those two objectives is (really) required.
At times - such 'optimization' produces 'unanticipated consequences' - such as, 'Optimizing AWAY certain elements (especially variables) of your code!' (i.e. that code and/or variable will then 'not' be 'acted upon!') You should note that the Compiler (in its considered {sometimes inflated} opinion) makes such decisions 'on its own' - and (rarely) informs/advises of such action! To be fair - there ARE coding practices you can adopt which, 'Limit such Compiler Intrusions.'
Your 'IDE' along w/some experimentation will increase your understanding of the various 'trade-offs' - resulting from each optimization level. Again - there is 'NO Universal Optimization Level' - ideal for 'each/every' MCU application & implementation. Often - it proves best to produce (otherwise) identical boards - but compiled w/different optimization settings - and then to provide sufficient 'operational time' to compare & contrast - which enables the recognition of 'best performer.'
Hello,
I think you may have posted to the wrong E2E forum. We have a Chinese forum that is available for you to use: https://e2echina.ti.com/
I think you'd be best of asking your questions there and getting support through that forum where other native speakers can best understand your question and provide feedback.
I will re-post this message with Google Translate in attempt to help you understand.
你好,
我想你可能已经发错了E2E论坛。 我们有一个中文论坛供您使用: https://e2echina.ti.com/
我认为您最好在那里提出问题并通过该论坛获得支持,其他母语人士可以最好地理解您的问题并提供反馈。
我将使用Google翻译重新发布此消息,以帮助您了解。