Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
Tool/software: Code Composer Studio
I am using CCS development tool on Hercules TMS570LC4357 development KIT. I am trying to write a code to send ADC reading to my PC. I followed the examples on ADC and SCI interface. I was able to read ADC and interface with SCI. However, when I try to combine the two project together by activating both ADC and SCI using HALCOGEN , I got errors in compilation like the following:
>> Compilation failure
source/subdir_rules.mk:9: recipe for target 'source/HL_can.obj' failed
"../source/HL_can.c", line 1657: error #20: identifier "CAN1_CTL_CONFIGVALUE" is undefined
"../source/HL_can.c", line 1658: error #20: identifier "CAN1_ES_CONFIGVALUE" is undefined
"../source/HL_can.c", line 1659: error #20: identifier "CAN1_BTR_CONFIGVALUE" is undefined
.....
There are bunch of this kind of errors on modules like DCC, EMIF, I2C etc. I am not using these modules. I don't know what I did wrong could you advice?
Thanks,
XG