Part Number: TM4C1294NCPDT
HI,
I am using TM4C1294NCPDT microcontroller, I have a slave IC configurable through I2C. Below is the piece of code I am ising to Configure and read ID from the slave.
void I2C_Init(){
//enable I2C module 1
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C1);
//reset module
SysCtlPeripheralReset(SYSCTL_PERIPH_I2C1);
//enable GPIO peripheral that contains I2C 1
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOG);
// Configure the pin muxing for I2C0 functions on port B2 and B3.
GPIOPinConfigure(GPIO_PG0_I2C1SCL);
GPIOPinConfigure(GPIO_PG1_I2C1SDA);
// Select the I2C function for these pins.
GPIOPinTypeI2CSCL(GPIO_PORTG_BASE, GPIO_PIN_0);
GPIOPinTypeI2C(GPIO_PORTG_BASE, GPIO_PIN_1);
// Enable and initialize the I2C1 master module. Use the system clock for
// the I2C1 module. The last parameter sets the I2C data transfer rate.
// If false the data rate is set to 100kbps and if true the data rate will
// be set to 400kbps.
I2CMasterInitExpClk(I2C1_BASE,(SysCtlClockGet()), true);
//clear I2C FIFOs
HWREG(I2C1_BASE + I2C_O_FIFOCTL) = 80008000;
}
uint32_t I2C_Read(uint8_t slave_addr, uint8_t reg)
{
uint32_t error = 0;
//specify that we are writing (a register address) to the slave device
I2CMasterSlaveAddrSet(I2C1_BASE, slave_addr, false);
//specify register to be read
I2CMasterDataPut(I2C1_BASE, reg);
//send control byte and register address byte to slave device
I2CMasterControl(I2C1_BASE, I2C_MASTER_CMD_BURST_SEND_START);
//wait for MCU to finish transaction
while(I2CMasterBusy(I2C1_BASE));
error = I2CMasterErr(I2C1_BASE);
//specify that we are going to read from slave device
I2CMasterSlaveAddrSet(I2C1_BASE, slave_addr, true);
//send control byte and read from the register we specified
I2CMasterControl(I2C1_BASE, I2C_MASTER_CMD_SINGLE_RECEIVE);
//wait for MCU to finish transaction
while(I2CMasterBusy(I2C1_BASE));
//return data pulled from the specified register
return I2CMasterDataGet(I2C1_BASE);
}
Slave address is 0xCE, when i pass this as argument to the read function I was not getting ID read, so probed the SCL and SDA lines.
Found that slave address as captured by scope is 0x9C but what I am configuring is 0xCE. So, slave might not be acknowlidgening.
Pull ups are present and SCL/SDA appears clean.
Is there any issue with the code posted above? Where am I missconfiguring the bus?
Thanks,
Janardan