Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C123GH6PM: TM4C123 Evaluation Board Periodic Timer not Working

Part Number: TM4C123GH6PM
Other Parts Discussed in Thread: EK-TM4C123GXL

I am starting to learn how to use timers/interrupts on the TM4C123 evaluation board (TM4C123GH6PM MCU).
In this example I am configuring a timer to create 1 second delays to toggle an on-board LED on and off. But when I run the code in real time on the board, the red LED appears to be on all the time. If I step through the code with breakpoints in my `while(1)` loop where I poll the timer register, it appears to work fine. (I am not using interrupts with this timer, just polling). 
I haven't attached the individual register breakdowns from the datasheet as there are quite a few.
Has anyone got any ideas as to why this is not working as expected?
Below is my code for the example I am following from the TM4C123 datasheet:
And here is my code:
         #include "include/tm4c123gh6pm.h"
         #define RED_LED (1U << 1)
         #define BLUE_LED (1U << 2)
         #define GREEN_LED (1U << 3)
       
         int main()
         {
          SYSCTL_RCGCGPIO_R = 0x20U;              //Enabling clock to port F.
          GPIO_PORTF_LOCK_R = 0x4C4F434BU; //Unlocking the port F lock register.
          GPIO_PORTF_CR_R = 0xFFU;                  //Enabling the port F commit register.
          GPIO_PORTF_DIR_R = 0x0EU;                 //Setting the port F pins as outputs.
          GPIO_PORTF_DEN_R = 0x1FU;                //Enabling digital writing to port F.
          
          
        /* To use a GPTM, the appropriate TIMERn bit must be set in the RCGCTIMER or RCGCWTIMER
          register (see page 338 and page 357). If using any CCP pins, the clock to the appropriate GPIO
          module must be enabled via the RCGCGPIO register (see page 340). To find out which GPIO port
          to enable, refer to Table 23-4 on page 1344. Configure the PMCn fields in the GPIOPCTL register to
          assign the CCP signals to the appropriate pins (see page 688 and Table 23-5 on page 1351). */
          
          SYSCTL_RCGCTIMER_R = 0x01U;  //Enable timer 0 clock signal.
          
        /* 1. Ensure the timer is disabled (the TnEN bit in the GPTMCTL register is cleared) before making
          any changes. */
       
          TIMER0_CTL_R &= ~(1<<0);   //Disabling timer.
          
        /* 2. Write the GPTM Configuration Register (GPTMCFG) with a value of 0x0000.0000. */
         
          TIMER0_CFG_R = 0x00000000U;  //Writing 0 hex to this register.
          
          
        /* 3. Configure the TnMR field in the GPTM Timer n Mode Register (GPTMTnMR):
          a. Write a value of 0x1 for One-Shot mode.
          b. Write a value of 0x2 for Periodic mode. */
       
          TIMER0_TAMR_R |= (0x2<<0);  //Setting timer 0 to periodic mode.
          
   
    /*  4. Optionally configure the TnSNAPS, TnWOT, TnMTE, and TnCDIR bits in the GPTMTnMR register
      to select whether to capture the value of the free-running timer at time-out, use an external
      trigger to start counting, configure an additional trigger or interrupt, and count up or down. */
      
      TIMER0_TAMR_R &= ~(1<<4);   //Configured as count down timer.
      
    /*  5. Load the start value into the GPTM Timer n Interval Load Register (GPTMTnILR). */
      
      TIMER0_TAILR_R = 0x00F42400; //16,000,000Mhz clock,  1 sec delays.
      
    /* 6. If interrupts are required, set the appropriate bits in the GPTM Interrupt Mask Register
      (GPTMIMR). */
      
      //Interrupts are not used, I am polling the timer0 regsiter as seen below in while(1) loop.
      
    /*  7. Set the TnEN bit in the GPTMCTL register to enable the timer and start counting. */
   
      TIMER0_CTL_R |= (1<<0);    //Enabling timer
      
    /*  8. Poll the GPTMRIS register or wait for the interrupt to be generated (if enabled). In both cases,
      the status flags are cleared by writing a 1 to the appropriate bit of the GPTM Interrupt Clear
      Register (GPTMICR). */
      
      while(1)
      {
       if( (TIMER0_RIS_R & 0x00000001) == 1) //Checking if timer has finished counting.
       TIMER0_ICR_R |= (1<<0);        //Clearing the finished timing bit in TIMER0_RIS_R.
       GPIO_PORTF_DATA_R ^= (1U << 1);    //Toggling the RED_LED output. 
      }
     }
 
 
  • Please use the TivaWare library functions to configure the timer. It will greatly reduce the complexity of configuring the timer and therefore reduce the number of coding errors. I suggest you look at the example in the TivaWare library: C:\ti\TivaWare_C_Series-2.1.4.178\examples\boards\ek-tm4c123gxl\timers

  • As the vendor agent advises - you've chosen among (if not) the, 'Hardest, Longest, & Most Error-Likely' Programming vehicle.      Vendor's 'painstakingly created API insures that your code 'meets deadlines' - and has the best chance to run & maintain robustness.

    Two elements of your 'Direct Register' code concern:

    • are you sure that you are employing the 'FULL' rather than 'HALF' Timer?     If the Timer is 32 bits - and set to 'Half' - then loaded w/ '16,000,000' - it cannot function per your intent.    (Half Timer accepts up to ~65K - when the Full-Timer is sized 32 bits.)
    • you check for 'timer completion' with a 'too severe' comparison!
      • if( (TIMER0_RIS_R & 0x00000001) == 1)    changing that ending parameter to <=1 (normally) will save you.   (provided the Timer does not roll-over)
      • to reduce (ideally eliminate) the impact of timer roll-over - add 1000 to your Timer Load register - and then test against <=1000.

    In the 'dark ages' we were forced to 'Do Battle' w/pages & pages of arcane MCU registers.     Today - the economy is Global - the Race is to the Swift - and only those (tenured/ensconced) w/in 'ivory towers' - force DRM (or worse ASM) upon their hapless subjects...    (some have said (I'm told) that 'job security' trumps 'student coding efficiency' - you should form your own conclusion...)