Part Number: TM4C123BH6ZRB
Hi, the sampling rate on the TM4C123BH6ZRB is 1 million samples/second. Can the sampling rate be configured or slowed down?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TM4C123BH6ZRB
Hi, the sampling rate on the TM4C123BH6ZRB is 1 million samples/second. Can the sampling rate be configured or slowed down?
Thanks!
Hello Bob,
Staff just noted and now states & then asks, "Indeed the Timer Trigger provides extreme flexibility in dialing-in the ADC's 'Sample Rate.' (that's 'just' as you've noted.)
However:
More clearly - I believe they are asking, "Can the time between successive ADC Acquisitions - during a 'Multi-Stepped Acquistion Sequence' - be somehow controlled? And of course ... if so ...how?
Thank you for your insights - as always - much appreciated.
What version of TivaWare uses this function? I do not have it in TivaWare-SW-TM4C-2.0.1.11577.exe
Thanks,
Joe