Hello Team,
I am working with a customer whom i am trying to provide some information regarding the following. Can you provide some guidance on where to start? He is trying to implement a 25 pin serial interface RS422 or RS232.
2) Determine if the built in TIVA-C serial controllers can support the desired protocols or do we need an external synchronous serial controller for the desired protocols? Our baud rate is 38.4Kbps and below. (25 pin serial port would support being configured via software to either RS422 or RS232)
3) If there is code available I know who would like to see it.