Part Number: TMS570LS1227
Other Parts Discussed in Thread: HALCOGEN
Hi,
we have another problem here with the uart running in the het. When receiving blocks of data back to back it seems to be losing synchronisation after a while. So in a block of 256 bytes after about 150ish bytes there are only incorrect bytes being received. One byte is always missing.
So can somebody confirm / deny if the ti het uart emulation can operate at 57600baud with a VCLK2 of 48MHz and an LRPFC of 64? I get a figure of 57692baud so in theory there should not be any characters being lost.
Regards,