Other Parts Discussed in Thread: ENERGIA
Hi,
I need to access PA0 and PA1 pins of the eval board for GPIO purposes. However I could not find the pins PA0, PA1, PD4 and PD5 on the evaluation board.
In the Energia diagram i have attached, below these 4 pins are grouped together. It also says these pins form the UART communication pins.
1) Does it mean I cannot use them on the launch pad?
2) If I can use them for GPIO purposes, are they broken out on the launchpad?
Thanks
BS