This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TM4C1294NCPDT: Chip bootloader upgrade to serial port

Part Number: TM4C1294NCPDT


Hi Ti Tema:

I use TI TM4C1294NCPDT, and I have the following problems. Please give me some Suggestions. Thank you.

Can the IC upgrade bootloader into a serial port?

BR

Sunny

  • Hello Sunny,

    If I am understanding right, you want to understand what boot loader capabilities the device has for serial ports such as UART?

    If so, there are two options:

    1) Use the ROM Boot Loader for the device, which can be used either when the device Flash is empty or with a TivaWare API

    2) Use a Flash boot loader such as the boot_serial boot loader with boot_demo1 and boot_demo2 examples provided in TivaWare.

    TivaWare can be downloaded from: http://www.ti.com/tool/sw-tm4c