Tool/software: Code Composer Studio
Hello ,
I tried to run HALCoGen (example_hetPwm.c) as a study project.
But It doesn't work, the oscilloscope shows no signal , could anyone help??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hello ,
I tried to run HALCoGen (example_hetPwm.c) as a study project.
But It doesn't work, the oscilloscope shows no signal , could anyone help??
Hello Miro,
I had tested the code to generate a PWM signals with a 80 MHz and different periods (900 µs ,999 µs ) and 50% duty cycle on HET1 pin 8. it shows the accurate measurements on oscilloscope.
but if i increase the periods to above of 999µs (1ns,10ns ,....) it shows incorrect measurments.
do you know the maximum range i can reach? do i need to change the frequency ?
Best Regards,