Part Number: TMS570LS0432
I need to implement watch dog timer in my code. I initialized for 100ms as:
rtiREG1->WWDSIZECTRL = 0x00000005;
rtiREG1->DWDPRLD = 0x3D1;
rtiREG1->DWDCTRL = 0xA98559DA;
In the main code, i'm setting WDKEY at the starting of the function as:
rtiREG1->WDKEY = 0xE51A;
& setting it again as
rtiREG1->WDKEY = 0xA35C; when a corresponding function is finished it's task.
When i ran the code, i NERROR LED is flashing. I removed the WD function & flashed the code, controller is working fine.
Can anybody help me on whether the sequence for enable & servicing the watch dog is correct.