Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
Tool/software: Code Composer Studio
I need codes for HET_PWM to control spark timing. There are 60-2 (2 teeth missing or removed) teeth on the circular disc called trigger wheel. After crossing 58 teeth pulse, the signal is sensed by Position sensor is supplied to HET1_18 pin. Then the received signal with few milli second time is send to timer IC through HET1_12 pin.
Kindly send the codes for the above conditions.