Part Number: EK-TM4C129EXL
hello,
unfortunately, I can not find an example showing the use of the RTC module in TI-RTOS.
I only found the hibernation example without TI-RTOS.
I have installed this in a function in TI-RTOS.
That's how it works. When I wrap the file for the hibernation module #include <driverlib / hibernate.h>, I get the warning: 233-D declaration is not visible outside of function.
Can I use the RTC from the Hibernation module in Ti-RTOS?
Are there any better ways to use an RTC?
I have an external clock of 32,768kHz on XOSC0 / 1.
Here is my code under TI-RTOS in the file TM4C129EXL.c:
#include <driverlib/hibernate.h>
void EK_TM4C129EXL_initHibernateMode(void)
{
SysCtlPeripheralEnable(SYSCTL_PERIPH_HIBERNATE);
HibernateEnableExpClk(SysCtlClockGet());
HibernateClockConfig(HIBERNATE_OSC_LOWDRIVE);
HibernateRTCEnable();
HibernateCounterMode(HIBERNATE_COUNTER_RTC);
uint8_t i;
for (i = 0; i < 100; ++i)
{
uint32_t secdec = HibernateRTCSSGet() * 1000/32768; // secdec ist 0.xx Sekunden
System_printf("%d\n", secdec); System_flush();
}
if(HibernateIsActive())
{
_nop();
}
else
{
_nop();
}
}